Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Error message occurs in update of CubeSuite+ by using Update Manager.

Latest Updated:12/14/2012

Question:

When I try to update the CubeSuite+ by using the Update Manager, I get the following error message and the installation fails:

M0120001
Installation is suspended because "CubeSuite+W.exe" is running.
It will be resumed next time you start the tool.

Answer:

Is not your CubeSuite+ launched by enabling rapid startup?
If it is not, exit it once and then run the Update Manager.
Suitable Products
CS+ (formerly CubeSuite+)