Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Inputting and Holding Reset Signal Active for a Long Time

Last Updated:05/25/2018

Question:

Is it OK to input and hold the reset signal active for several seconds?

Answer:

A long reset will not pose any problem.
While a minimum length is specified for the reset signal, no maximum length is specified.
In other words, a long reset will not cause any problem.
Suitable Products
RL78/G10
RL78/G11
RL78/G12
RL78/G13
RL78/G14
RL78/G1A
RL78/G1C
RL78/G1D
RL78/G1E
RL78/G1F
RL78/G1G
RL78/G1H
RL78/I1A
RL78/I1C
RL78/I1D
RL78/I1E
RL78/L12
RL78/L13
RL78/L1A
RL78/L1C
78K Family