Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Do the products of Renesas Electronics regulated by RoHS Directive?

Latest Updated:11/01/2008

Question:

Do the products of Renesas Electronics contain substances regulated by the RoHS Directive?

Answer:

The only substance in Renesas Electronics products that exceeds the reference levels prescribed by the RoHS Directive is lead (Pb) in old solder plated products. Therefore, lead-free products comply with the RoHS Directive.
Renesas Electronics performs in-process control for six substances restricted by the RoHS Directive, and our lead-free products are also verified to have lower lead levels than the RoHS reference value.
Renesas Electronics promotes the transition to lead-free products according to the green procurement aims.
Suitable Products