Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is supply of a PLP product assured for the stated supply period?

Latest Updated:04/01/2015

Question:

Is supply of a PLP product assured for the stated supply period?

Answer:

The PLP is not a guarantee of supply. The program provides information on Renesas' planned supply period for a product as reference for users who are considering using the product.
Renesas is also a manufacturer, and thus purchases materials, equipment, and so on from external sources. If an upstream supply issue occurs and no alternative means can be found, this would affect our supply period. That is why information on the PLP period must be viewed as reference only. If Renesas has to shorten a PLP period due to the aforementioned factors, Renesas will issue a PDN (Product Discontinuance Notice) in accordance with JEDEC (JESD48B), and supply will be continued for 24 months from the date of EOL announcement.
Suitable Products
PLP (Product Longevity Program)