Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What does the (0) affixed to some transistor or FET order numbers mean?

Latest Updated:07/01/2006

Question:

What does the (0) affixed to some transistor or FET order numbers mean?

Answer:

(0) is an automotive electronics compliance symbol and means that the product is a high-quality, high-reliability product suitable for automotive applications.
Suitable Products