Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What is the APP value of Renesas Electronics' microcontrollers?

Latest Updated:02/01/2008

Question:

Under Japanese export controls, the measure of performance of digital electronic computers has changed from "Composite Theoretical Performance (CTP)" to "Adjusted Peak Performance (APP)," but what is the APP value of Renesas Electronics' microcontrollers?

Answer:

Renesas Electronics recommends the use of the estimated value of adjust peak performance (APP) for judging whether a given product is subject to export control restrictions.
The APP estimated value for 64-bit and 32-bit microcontrollers is 0.01 WT (Weighted Tera FLOPS).
In the case of microcontrollers of 16 bits or less, the estimated value is 0 WT because such products do not have functions that execute floating point operand operations.
Suitable Products
  • Was this article helpful?