Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is the function of H8S/2322 valid for clock synchronous operation?

Latest Updated:03/18/2009

Question:

For the H8S/2322 to select data logic level reverse requires setting SCMR SINV bit to 1 in normal operation (SCMR SMIF is 0). Is this function valid for clock synchronous operation ?

Answer:

Yes, it is also vaild for clock synchronous operation
Suitable Products
H8S Family