Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Any specifications for external capacitor that is connected to port?

Latest Updated:02/27/2012

Question:

Are there any specifications for the external capacitor that can be connected to the port?

Answer:

The value of the external capacitor is not specified. However, when shutting down the MCU power please note that the voltage applied to the port should not be higher than the power supply voltage.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N