Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Are serial and other port settings required during flash programming?

Latest Updated:12/01/2011

Question:

Are serial and other port settings required during flash programming?

Answer:

Settings are not required.
When the flash programming mode is set, the internal firmware performs the settings that are required for programming, so it is OK to just connect the signal used for programming to the programmer.
Suitable Products