Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Are the H8/300H series Flash devices in circuit programmable ?

Latest Updated:03/18/2009

Question:

Are the H8/300H series Flash devices in circuit programmable ?

Answer:

All Renesas flash micro-controllers can be programmed in circuit. Each device comes with a built in boot loader which allows the device to be programmed automatically from a host computer via the on-chip serial port. Full details of this can be found in the users manuals of each device.
Suitable Products
H8/300H
H8/300H Tiny