Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Are there any SFRs that must not be read out in addition to address 0h?

Latest Updated:03/15/2012

Question:

Are there any other SFRs that must not be read out in addition to address 0h?

Answer:

Yes. Reading from/writing to addresses which nothing is assigned (reserved) in the SFR area is inhibited.
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N