Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Are there any products similar to M16C Flash Starter?

Latest Updated:03/01/2005

Question:

(Flash Memory)   I would like to perform on-board programming. Are there any products similar to M16C Flash Starter? [2005/03/01]

Answer:

The M16C Flash Starter supports some of the 8-bit MCUs. For more details concerning supported products, please click here. (#104887)
Suitable Products
3803H
3803L
3850A
38D2
38D5
M3A-0806