Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Are there any products which incorporate the main oscillator?

Latest Updated:03/26/2009

Question:

Are there any products which incorporate the main oscillator?

Answer:

Yes, there are.
Suitable Products
H8/300H Tiny
H8/36109
H8/36077, H8/36079
H8/36912, H8/36902