Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can I change the transfer mode during repeat transfer mode operation?

Latest Updated:03/15/2012

Question:

Can I change the transfer mode during the repeat transfer mode operation?

Answer:

No, you should not change the transfer mode during the DMA transfer. You need to disable the transfer operation before changing the transfer mode. Changing the transfer modes without disabling transfer operation may cause improper data transfer.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A