Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can I use 32kbyte when using E7 by H8/38024 or H8/38004 F-ZTAT version?

Latest Updated:03/25/2009

Question:

When using the E7 by H8/38024 or H8/38004 F-ZTAT version, can I use 32kbyte of ROM?

Answer:

No, you can use only 28kbyte of ROM since E7 uses 4kbyte of ROM for HDI monitor.
Suitable Products
H8/300L Super Low Power
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3802, 38002S, 38004, 38104
H8 Super Low Power