Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can I use WDT on an H8/300H Tiny device as an interval timer?

Latest Updated:03/26/2009

Question:

Can I use WDT on an H8/300H Tiny device as an interval timer?

Answer:

No, you can't.
Suitable Products
H8/300H Tiny
H8/36109
H8/36077, H8/36079
H8/36064
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3672
H8/3664