Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can TxDi pin used as an I/O port if transmission is performed in UARTi?

Latest Updated:09/22/2010

Question:

When only transmission is performed using serial interface UARTi, can the RxDi pin used as an I/O port?

Answer:

The RxDi pin can be used as an I/O port.
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/65
M16C/6C
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A