Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can a program which developed as M38039FFFP be used as M38039FFHFP?

Latest Updated:10/19/2004

Question:

(Migration)   Can a program which was developed as M38039FFFP (standard) be used as M38039FFHFP (Spec.H)? [2004/10/19]

Answer:

Program modifications when switching from standard to Spec.H are not necessary.
However, since the flash memory type of standard and Spec.H in CPU rewrite mode differ, program modifications are necessary. (#104926)
Suitable Products
3803H
3803L