Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can the H8S/2357 DMA controller transfer word data from 8 bit to 16 bit?

Latest Updated:03/18/2009

Question:

Can the H8S/2357 DMA controller transfer word data from an 8bit access area to a 16bit access area ?

Answer:

Its possible to transfer word data from an 8bit access area to a 16bit access area. Select Word size transfer by setting the DMA control register (DMACR) DTSZ bit to 1.
Suitable Products
H8S Family
  • Was this article helpful?