Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can the watchdog timer be stop if it started counting after a reset?

Latest Updated:03/01/2005

Question:

(Watchdog Timer)  If the watchdog timer started counting due to a write to the watchdog timer control register after a reset, can it be stopped by software? [2005/03/01]

Answer:

No, it cannot.
The watchdog timer is stopped after a reset. Writing to the watchdog timer control register will start the count. The only way to stop the count once it has started is to reset. (#104849)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544