Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Do I have to keep the table area corresponding to unused interrupt free?

Latest Updated:03/19/2017

Question:

Do I have to keep the table area corresponding to unused interrupts free?

Answer:

No, you don't.
This memory area is reserved only for interrupts.
If you do not use an interrupt, the corresponding area can be used as a normal memory area.
Suitable Products
V850 Family