Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Do RTOS (uITRON) products include a TCP/IP protocol stack area?

Latest Updated:12/01/2011

Question:

Do RTOS (uITRON standard) products include a TCP/IP protocol stack area?

Answer:

The V850 Series supports TCP/IP (product name: AP703100-B17).
The following third-party products are also provided:

- AI Corporation
- ACCESS CO., LTD.
- Aplix Corporation
- Elmic Systems Inc.
Suitable Products