Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Do restrictions for 7540 Group apply to the 7542, 7546 and 7547 Group?

Latest Updated:09/29/2006

Question:

(Serial Interface)  Do any of the following restrictions for the 7540 Group apply to the 7542, 7546 and 7547 Group? [2006/09/29]
Usage conditions for serial I/02
・ When serial I/01 is not in use
・ When serial I/01 is used as UART and divide-by-16 of BRG
output is selected for the synchronous clock

Answer:

Neither of these restrictions apply to the 7542, 7546 and 7547 Group. (#104930)
Suitable Products
7546
7547