Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Does DTC activate immediately while CPU executes interrupt handling?

Last Updated:12/26/2017

Question:

When a DTC activation source is generated while the CPU executes interrupt handling, is the DTC activated immediately, after interrupt handling is completed, or depending on the priority order of interrupt sources?

Answer:

The DTC is activated immediately. The DTC and CPU use the same bus, and the DTC takes priority over the CPU in using the bus. The DTC takes priority regardless of the priority of interrupt sources.
Suitable Products
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32M
R8C/33M
R8C/34M
R8C/35M
R8C/36M
R8C/38M
R8C/3GM
R8C/3JM
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
R8C/L35M
R8C/L36M
R8C/L38M
R8C/L3AM