Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Does the product packaged with a write control for a serial programmer?

Latest Updated:03/01/2005

Question:

(Flash Memory)   Does the product come packaged with a write control program for a serial programmer? [2005/03/01]

Answer:

Yes. The write control program for a serial programmer is stored in the boot ROM area.
If you plan on using a serial programmer, be careful not to erase the boot area by mistake when reprogramming with a parallel programmer. (#104876)
Suitable Products
3803H
3803L
3850A
38D2
38D5