How can I output a clock signal?
Latest Updated:03/24/2009
Question:
How can I output a clock signal?
Answer:
There are several ways as below.
1. Use PWM
2. Use toggle output of timer
3. Use TMOW pins (its availability depend on each product)
4. Use SCI1 clock continuous output mode 4 (its availability depend on each product).
For detailed, please refer to the hardware manual.
Suitable Products
H8/38602R |
H8/38086R |
H8/38086 |
H8/38076R |
H8/300L Super Low Power |
H8/3887 |
H8/3867 |
H8/3857 |
H8/3854F |
H8/3854 |
H8/38024R, 38024, 38024S, 38124 |
H8/38024F |
H8/3824 |
H8/3802, 38002S, 38004, 38104 |