Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to adjust the luminance in H8/3802, H8/38004 and H8/38024 Groups?

Latest Updated:03/25/2009

Question:

I'd like to know how to adjust the LCD panel's luminance in the H8/3802, H8/38004 and H8/38024 Groups.

Answer:

Please adjust the luminance by inserting a variable resistor between Vcc and V1. Since driving power is supplied externally, please set PSW bit to 0.
Suitable Products
H8/300L Super Low Power
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3802, 38002S, 38004, 38104
H8 Super Low Power