Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to find Icc for frequencies that are not included on ECT?

Latest Updated:03/13/2008

Question:

(Electrical Characteristics)  How can I find the Icc for frequencies that are not included on the Electrical Characteristics Table? [2008/03/13]

Answer:

Click the Group of your MCU.

Click:
3823    38D2    38D5   3803H   3850A
7542   7545   7546   7547    7548    7549

Standard characteristics are listed on the above pages.
Standard characteristics are example measurements of standard samples. They are provided for reference only and are not guaranteed.

(#106391)

Suitable Products
3803H
3803L
3823
3850A
38D2
38D5
7545
7546
7547
7548
7549