Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

In what situation is the flash memory reset bit used?

Latest Updated:03/01/2005

Question:

(Flash Memory)   In what situation is the flash memory reset bit used? Also, can I use the read command to terminate other commands in process? [2005/03/01]

Answer:

The flash memory reset bit is used to safely terminate the erase and program commands. To terminate a command in process, set the bit to "1" (reset), then set it again to "0" (normal operation). (#104868)
Suitable Products
3803H
3803L
3850A
38D2