Is 1.5mA an acceptable current while the DAi pin is outputting 0V?
Latest Updated:03/01/2005
Question:
(D/A Converter) Is 1.5mA (peak) an acceptable current while the DAi pin is outputting 0V ? [2005/03/01]
Answer:
There is no problem with 1.5mA current flow itself. However, please keep in mind that D/A output precision will be greatly reduced while current is flowing. (#104838)
Suitable Products
3803H |
3803L |