Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is full duplex communication possible with UARTi of the R8C Family?

Latest Updated:09/17/2010

Question:

Is full duplex communication possible with the serial interface (UARTi) of the R8C Family?

Answer:

Yes, it is possible.
Suitable Products
R8C/1x
R8C/2x
R8C/3x
R8C/Lx
R8C/Mx