Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is it possible to modify chip contents if protection is enabled?

Latest Updated:08/05/2009

Question:

(Flash Memory)
1.   In the Flash version, is it possible to read out or modify the chip contents when protection is enabled?
2.   Also, is it possible to erase the chip contents even if the ID code doesn't match? [2009/08/05]

Answer:

  1. In standard serial I/O mode, Flash chip contents can be safely protected from being read out, rewritten, or erased by setting an ID code. In parallel I/O mode, they can be protected using the ROM code protect function.
  2. No, the chip contents cannot be erased if the ID code doesn't match.

(#107431)

Suitable Products
3803L
38D2
38D5