Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is it possible to use Advantest R4945 and Renesas programming adapter?

Latest Updated:12/07/2004

Question:

(Flash Memory)   EFP-I by Suisei Electronics System Co., Ltd. is recommended as a flash memory programmer for 3803 (Spec.H).
I would like to use the Advantest R4945 and Renesas programming adapter, as I do for the standard product. Is this possible? [2004/12/07]

Answer:

Since the flash memory specifications of Spec.H differs from that of the standard product, the Advantest R4945 + Renesas programming adapter combination cannot be used. (#104934)
Suitable Products
3803H
3803L