Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is there a guaranteed operating humidity level for Flash ROM?

Latest Updated:03/12/2008

Question:

Is there a guaranteed operating humidity level for Flash ROM?

Answer:

No, we do not provide a regulation guaranteed operating humidity level. However, we recommend an operating environment of 40%-80%. In addition, it is advisable to avoid use in an environment in which condensation would be able to form.
Suitable Products
H8S/2678, 2678R
H8S/2668
H8S/2649
H8S/2648, 2646
H8S/2643
H8S/2630, 2639, 2638, 2636, 2635
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2609
H8S/2607
H8S/2604
H8S/2602
H8S/2556, 2552, 2506
H8S/2472, 2463, 2462
H8S/2378, 2378R
H8S/2368
H8S/2398, 2357
H8S/2345
H8S/2339
H8S/2329
H8S/2319
H8S/2282, 2280
H8S/2268, 2264
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2218, 2212
H8S/2199R
H8S/2194
H8S/2189R
H8S/2172
H8S/2168
H8S/2169, 2149
H8S/2164
H8S/2158
H8S/2153
H8S/2148, 2144
H8S/2144B,2134B
H8S/2140B
H8S/2138, 2134
H8S/2125
H8S/2128, 2124
H8S/2117, 2117R
H8S/2116
H8S/2114R
H8S/2111B
H8S/2110B
H8SX/1720S (H8SX/1720, H8SX/1720S)
H8SX/1668R, H8SX/1668M
H8SX/1663
H8SX/1658R, H8SX/1658M
H8SX/1657
H8SX/1653
H8SX/1648A, H8SX/1648L
H8SX/1638, H8SX/1638L
H8SX/1622
H8SX/1580
H8SX/1568
H8SX/1558
H8SX/1544
H8SX/1520R