Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is there any package corresponding to H8/3664N with on-chip EEPROM?

Latest Updated:03/26/2009

Question:

Is there any package corresponding to H8/3664N with on-chip EEPROM?

Answer:

FP-64E is the only available package for H8/3664N.

Suitable Products
H8/300H Tiny
H8/3694
H8/3687
H8/3664