Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is there any tool to erase all data in Flash memory and reset the ID code?

Latest Updated:02/27/2012

Question:

Is there any tool to erase all data in Flash memory and reset the ID code, when I programmed any ID code and it is now unknown?

Answer:

No, there is not. To reprogram the Flash memory by serial programmer, the ID code already programmed in the MCU should match the one to be entered by the programmer. If the ID code programmed lastly is unknown and cannot be identified, it is impossible to reprogram the Flash memory by serial programmer.

However, when the ROM code protect function is not used, it is possible to reprogram it regardless of the ID code with a parallel programmer.

Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N