Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is there disparity in MCU current consumption among 2 methods for pins?

Latest Updated:01/09/2009

Question:

(I/O Port, Electrical Characteristics)  Is there a difference in MCU current consumption between the following two termination methods for unused pins in STOP mode:"Set to output mode and leave them open" and "Set to input mode and connect to VCC/VSS through resistor"? [2009/01/09]

Answer:

No, there is no difference in current consumption between the two methods. (#107248)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549