Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

MODE pin state when reset is deasserted, user program/standard serial I/O

Latest Updated:10/06/2016

Question:

When running a user program or in standard serial I/O mode, what is the effect of the state of the MODE pin when reset is deasserted?

Answer:

For the R8C Family, the operating mode depends on the state of the MODE pin when reset is deasserted, as shown below.

- When reset is deasserted when the MODE pin is at high level
  Mode: Single-chip mode
  Operation: Program runs on flash memory

- When reset is deasserted when the MODE pin is at low level
  Mode: Standard serial I/O mode
  Operation: Possible to rewrite user ROM area

For the detailed timing for transitioning to standard serial I/O mode, see section 5.1 Deciding Communication Format on page 50 of application note R01AN1469EJ0120 Rev.1.20 (R8C/38C Group Serial Programmer Using Standard Serial I/O Mode).

Suitable Products
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/32M
R8C/33M
R8C/34M
R8C/35M
R8C/36M
R8C/38M
R8C/3GM
R8C/3JM
R8C/33T
R8C/3JT
R8C/3NT
R8C/36T-A
R8C/38T-A
R8C/3MK
R8C/34K
R8C/3MU
R8C/34U
R8C/3MQ
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
R8C/L35M
R8C/L36M
R8C/L38M
R8C/L3AM
R8C/LA3A
R8C/LA5A
R8C/LA6A
R8C/LA8A
R8C/Mx