Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Other than RAM backup mode, is it okay to input valid wave forms to pins?

Latest Updated:07/04/2003

Question:

(Power Save)  In modes other than RAM backup mode, is it okay to input valid waveforms to pins that are always set for the key-on wakeup function?

Answer:

No problem. The key-on wakeup function is enabled only in RAM back-up mode. (#105023)
Suitable Products
4286
4508
4509
4571