ROMless / Mask ROM versions: is this a dedicated WDTOVF# terminal?
Latest Updated:01/18/2008
Question:
In the manual, there's a combination WDTOVF#(FEW,EMLE) terminal; in the ROMless/Mask ROM versions, is this a dedicated WDTOVF# terminal?
Answer:
Yes, in the ROMless/Mask ROM versions it is a dedicated WDTOVF# terminal.
Suitable Products
H8S/2398, 2357 |
H8S/2345 |
H8S/2329 |
H8S/2319 |