Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Stop Mode: Why is consumption currently fluctuating at higher values?

Latest Updated:11/05/2008

Question:

(Power Save)   In stop mode, consumption current may fluctuate at higher values. Is there any reason for this? [2008/11/05]

Answer:

In stop mode, consumption current may increase in the following case:

  • The input pins are in floating state (level not fixed) because the unused input pins are in open state.

(#107006)

Suitable Products
7545