Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What are the settings needed in clock synchronous serial I/O mode?

Latest Updated:03/07/2012

Question:

When continuous receive mode is selected in clock synchronous serial I/O mode, what are the necessary settings when starting reception?

Answer:

  • Transmit enable bit = "1"
  • Receive enable bit = "1"
  • Read the Receive buffer register

Performing the above settings outputs or inputs the transfer clock, starting reception.

Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N