Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What happen if data is executed without stopping programmable timer?

Latest Updated:02/05/2009

Question:

(Timer)  What will happen if the data read instruction is executed without stopping the counter for the programmable timer? [2009/02/05]

Answer:

The counter value may not be read correctly. (#107258)
Suitable Products
4286