Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What happens if MSTP10 is set High during D/A conversion?

Latest Updated:03/18/2009

Question:

On the H8S/2328 what happens if MSTP10 is set High during D/A conversion and what is the effect on power consumption ?

Answer:

When the module stop bit is set, access to control registers is prohibited and the content of control registers and outputs are retained. The power consumption of the device will reduce as in module stop the clock supply to corresponding module is removed.
Suitable Products
H8S Family