Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What happens if VREF is set to Vcc?

Latest Updated:03/08/2012

Question:

The current consumption will increase. In order to avoid this, set the VCUT bit of ADCON1 register to "Vref not connected". Also, for products that have an on-chip D/A converter, set the DAi register to "00h" and disable the D/A output with the DACON register.

Answer:

The current consumption will increase. In order to avoid this, set the VCUT bit of ADCON1 register to "Vref not connected". Also, for products that have an on-chip D/A converter, set the DAi register to "00h" and disable the D/A output with the DACON register.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N