Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What happens if another interrupt request will generate?

Latest Updated:03/07/2012

Question:

For the condition when an interrupt routine A is already being serviced and the interrupt nesting is enabled: If an another interrupt request B with the same priority as A in service generates, will this interrupt routine B be serviced?

Answer:

No, it will not be serviced. This interrupt routine B will be serviced after completing the interrupt routine A.
After accepting the interrupt A, the value of the interrupt A's priority level select bits (ILVL0-ILVL2) enters into the processor interrupt priority level (IPL).If the interrupt flag is set to "1" in the interrupt routine of the interrupt A. The only interrupt with the higher priority than the IPL is accepted, so the interrupt B request with the same priority isn't accepted.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N