Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What is custom code?

Latest Updated:04/01/2006

Question:

What is custom code?

Answer:

Custom code is used to identify infrared remote control users. In the NEC format, this is a 16-bit code that is inserted before the data code.

Also refer to the following FAQ item: NEC format for infrared remote control [Common]
Suitable Products