Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What is needed to simulate communication functions using simulator?

Latest Updated:12/01/2011

Question:

What is required to simulate communication functions using a simulator?
Also, how can I generate input data.

Answer:

Either create 01 patterns using a 01 editor or create an input file by specifying the desired pin, data and timing in the input timing chart window.
Download the input file created above before performing simulation.
For further details, see "Input Timing Chart Editor Window" in the Simulator User's Manual.
Another possible method is to create an external part where the serial pin data input function is called as a function.
Suitable Products