Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What is the difference between the IE-78K0S-NS and the IE-78K0S-NS-A?

Latest Updated:12/01/2011

Question:

What is the difference between the IE-78K0S-NS and the IE-78K0S-NS-A?

Answer:

The IE-78K0S-NS features the addition of performance functions, and for this reason has been named IE-78K0S-NS-A.
Suitable Products
78K Family