Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What is the initial value of TxD pin when the TE bit of SCR is set to 1?

Latest Updated:03/25/2009

Question:

What is the initial value of TxD pin, when the TE bit of serial control register (SCR) is set to 1?

Answer:

When TE bit is set to 1, the initial value of TxD pin becomes high level automatically in the asynchronous and clock synchronous modes. However, it is necessary to set to 1 the SPC3 bit of the serial port control register (SPCR) before TE bit is set, when setting the TxD pin to output. Also, SCINV bit of the register has output data inversion function.
Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power